|
The development of creative and scientific mind |
|
| |
Users can build various robots in their mind with Bioloid kit not just following assembly. The creativity and scientific mind are developed by solving the problems and processing robot assembly. | |
| |
 |
Concept of modular types robot |
|
| |
According to professionalism is developed in the latest engineering field, and structure is bulky, object oriented (object oriented) method is trend that is introduced, these technique was generalized in software specially. Introduces these concept in robot and is improving compatibility and efficiency that construct robot between robot. | |
|
 |
| |
 |
Motion teaching and playback practice |
|
| |
Method that stores motion of robot and does it so that play is robot control system used much in industry spot. Can grasp necessity of Torque control while it is practicing and can learn concept of position control, speed control. | |
 | |
| |
 |
Logic power elevation through behavior control programming |
|
| |
Behavior control programming is a one of the program process that express how to achive the function of robot.
There are various things such as fatigue of motion of robot, output and perception of sound, perception of object, button or remote control, temperature and robot to base elements of control. Robot can promote logic power making algorithm that achieve by visual method using these factors. | |
|
 |
| |
 |
| |
 |
Microcontroller basis abstract studying of robot base |
|
| |
Bioloid expert kit is handling method that control robot by microcontroller level. You can understand circuit diagram of robot, and robot internal devices can grasp run principle using I/O port and A/D converter. | |
| |
 |
Robot drive with C-language |
|
| |
There is an educational course which makes programs using GCC(Ansi-C: freeware) in Bioloid expert kit. The students study the C-programming operating skill on the embedded board. | |
| |
 |
Robot control that use radio communication |
|
| |
Bioloid expert kit practices learns basic concept about PAN ( Personal Area Network ), and control robot in PC or remote control by radio communication using Zig-100 communication module. | |
 | |
| |
 |
Dainamixel control that use PC |
|
| |
Bioloid expert kit introduces method that control Dynamixel directly in PC. Below picture is a key map that control Dynamixel directly in PC using USB 2 Dynamixel devices had included in expert kit. | |
|
 |
| |
 |
Studying about vision |
|
| |
Bioloid expert kit is handling method that sends a letter video signal that transfer in camera that is threaded to robot by radio and marks this by real-time on screen of PC through USB(image processing). Furthermore, Analyze image data and learn to simple realization (Edge detection) routine(image realization). | |
|
 |
| |
 |
Walk algorithm that use station kinematics of machinery |
|
| |
Bioloid expert kit is treating contents that understand concept of station kinematics of machinery, and apply station kinematics of machinery in walk. | |
 | |